cancel
Showing results for 
Search instead for 
Did you mean: 

Guidelines on maximum length allowable on PDM microphone lines (MP23DB01HP)

YChri.3
Associate

Would like to check if there any recommendation on the acceptable length for PDM bus, using MP23DB01HP.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Peter BENSCH
ST Employee

Welcome, @YChri.3​, to the community!

Please keep in mind that the clock frequency on the single ended line is 1...3.25MHz and the maximum load capacity at the output is 100pF. Additional lines add capacity, which affects the signal quality, so that a detailed examination is necessary for lines longer than approx. 20cm. If necessary, the use of termination resistors could also be useful.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.