Question
using the Motion DI Library and getting hard fault at No source available for "quatErr2EulerErr() at 0x800671c"
Hi, have successfully used the library before on an L476, needed more processing power so porting the project to an F746, however, there is a hard fault when using the motion_DI library. breaking the fault don the error message is No source available for "quatErr2EulerErr() at 0x800671c"
the library is initialising, but not running in the main loop,
I have increased the stack sizes as well as changed processors. I have also started a new project from scratch and it is still not working. I am using Library version 1.1.0 on x-cube MEMS 1