MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Good night. I have a LIS2DH12TR over an ATSAML21E17B. I´m reading the values of axis (x,y,x) transforming the values to degres (from -90º to 90º) but I need degrees from 0 to 360. I have tested a lot of formulas but nothing. Any idea? Ty.

This is the configuration of accelerometer:// Enable Block Data Update lis2dh12_block_data_update_set(&dev_ctx, PROPERTY_DISABLE); // Set Output Data Rate lis2dh12_data_rate_set(&dev_ctx, LIS2DH12_ODR_100Hz); // Set full scale lis2dh12_full_scale_set...

Ja by Associate
  • 1913 Views
  • 3 replies
  • 0 kudos

Resolved! For sensorfile.box, how to use ble physical peripherals to transfer data to the computer when Android studio is used to simulate the smartphone platform? Does st have this ble physical peripheral for sale? Where can I find this equipment?

Can you describe in more detail the problem of running Android studio to simulate the smartphone platform? Can this method really be realized? Are there any detailed connection steps and suggestions? Can you give me some more specific suggestions. th...

Ljiah.1 by Associate II
  • 1433 Views
  • 1 replies
  • 0 kudos

Resolved! ST sensor identification - package marking code

Good day!I need help with ST part identification base on package marking code.It is accelerometer (or IMU), in LGA-12 package, marked with "14J", "UA" (picture attached).Thanks in advance!

0693W00000GZqwaQAD.jpg
kkoziy by Associate
  • 1909 Views
  • 1 replies
  • 0 kudos

LIS2DS12 high output noise

Hello,I have a LIS2DS12 accelerometer connected to an arduino MKR1000 through SPI.For my application I need to use the highest ODR of 6400 Hz, and 2g FS.In order to collect 1 s of acceleration data, I constantly pull data from the FIFO. I set the thr...

Avian.1 by Associate
  • 4411 Views
  • 5 replies
  • 0 kudos