MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to connect STEVAL-STWINKT1B to pc to monitor and save data?

Hi.I bought a STEVAL-STWINKT1B board, however I try to perform all the steps to be able to see the data collected by the sensors and I can't because I can't understand what I need to do. I just wanted to connect this board via usb to my pc , monitori...

Tiago F by Associate
  • 2225 Views
  • 2 replies
  • 0 kudos

Strange behavior with call to HAL_GPIO_ReadPin()

I am seeing some strange happenings using X-CUBE-MEMS software pack, which generates some code for user buttons, LED outputs, etc.I noticed the user button was always returning GPIO_PIN_SET even when it should be returning GPIO_PIN_RESETI make a call...

Resolved! Best way to program (pro mode) SensorTile.box ?

Hi,I'm trying to program the SensorTile.box (in Pro Mode), I've tested the available examples from Function Packages and they are working. The thing is when I create a new project for the SensorTile.box with CubeIDE then CubeMX, the BSP generated and...

0693W00000HpUN5QAN.png
RJoac.1 by Associate II
  • 2338 Views
  • 3 replies
  • 0 kudos

Resolved! Understanding VL53L3CX histogram data

Hi, I'm a little confused about the data that is returned by VL53L3CX sensor. Here's a video illustrating the data.I would expect the histogram to be a time-series of the return pulses, with position on the x-axis representing their arrival times (di...

dscdsc by Senior
  • 3815 Views
  • 6 replies
  • 0 kudos