MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LSM6DSM on SensorTile using SPI?

I would like to know what I am doing wrong or what register setting on the LSM6DSM that I missed setting?Using a sensorTile (STM32L476JG) that is connected to LSM6DSM. APB1 Clk = 16MHz.My settings are : My code is trying to read WHO_AM_I register on...

0693W00000KbYP9QAN.png
SWenn.1 by Senior III
  • 3258 Views
  • 7 replies
  • 0 kudos

Resolved! How to use X-Cube-MEMS1 library

Hello everyone,I want to use the LIS3MDL Magnetometer sensor in the picture with a NUCLEO-L053R8 board with an I2C interface.I want to set the sensor to output an Interrupt.My question is: Can I do this, using the Official X-Cube-MEMS1 library? Is th...

0693W00000Kb6R7QAJ.png
KKoc.1 by Associate
  • 1791 Views
  • 1 replies
  • 0 kudos

ISM330DLC issue with sensor hub output registers 13-18

Hello,I'm currently trying out different configurations of the ISM330DLC sensor hub. Everything works as expected as long as I don't configure it to read more than 12 registers. If I do try to use more than 12 registers, I get some unexpected output ...

yath by Associate
  • 1406 Views
  • 3 replies
  • 0 kudos

LSM6DSM Help?

Hello....I am trying to communicate with the above subject but I am not sure what CPOL and CPHA should be set to. STM uses MODE1 - 4 but SPI talks about MODE 0 - 1. I have the following basic code to just try and read the WHO_AM_I Register (0x15) w...

SWenn.1 by Senior III
  • 1172 Views
  • 1 replies
  • 0 kudos

Resolved! LSM6DSM vs LSM303 threshold

I want to set a certain threshold on an accelerometer and have it generate an IRQ. Do both of these accelerometers allow me to do this?Is one better than the other for this application and if so why?Thank you

SWenn.1 by Senior III
  • 1465 Views
  • 1 replies
  • 0 kudos

Can Vl53l0x be use in outdoor environments?

I want to use the sensor in on of out devices to measure the obtacle in a given threshold range and was wondering if it can be used outdoors, how about covering this sensor with some coated glass ? will that work? Please suggest so we can finalize ...

SChau.11 by Associate
  • 1894 Views
  • 1 replies
  • 0 kudos