MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Magnetometer Offset Cancellation

Hello, I am trying to figure out if disabling the Offset Cancellation on the LSM303AGR would impact the wake up trigger mechanism. From what I could find, the LSM303AGR is an AMR sensor that uses the magneto-resistant property of a film to change its...

Resolved! ISM330BX datasheet error. In AN6109 (device application note)

anyone know who to contact about an error in the datasheets? In the AN6109 (device application note) of the ISM330BX datasheet on page 65/107 in section 8.2 FIFO registers there are three line I believe have errors: – SFLP_GBIAS_FIFO_EN bit of the EM...

no by Associate
  • 472 Views
  • 1 replies
  • 0 kudos

Build fails on NUCLEO-WBA55CG after enabling X-CUBE-MEMS

Hello,I have been working with a NUCLEO-WBA55CG board and the X-NUCLEO-IKS02A1 expansion board. I am running into an issue where the project fails to build after I enable the X-CUBE-MEMS software pack.Here are the steps to reproduce the problem:In ST...

kclauah by Associate II
  • 706 Views
  • 6 replies
  • 2 kudos

Resolved! Is X-CUBE-MEMS1 supported on STM32N6

So i'm trying to install X-CUBE-MEMS1 in the IOC file of a STM32N6-DK board.  The problem i can't seem to install it?  All the tabs are greyed out and have little red cpu marks by them.  Is X-CUBE-MEMS1 supported on STM32N6 processors?   When i go to...

Screenshot from 2025-11-17 12-20-46.png

FIFO data in Stream-to-FIFO mode

Hi,It's mentioned in the datasheet that the sensor will convert the FIFO from streaming (reading data all the time) into FIFO (holding the data until it's read) If i am getting it right, then my question isWhen exactly will the sensor read ? Will it ...

abduuu by Associate II
  • 432 Views
  • 2 replies
  • 0 kudos

Sensing total acceleration LIS2DH12

I was asking can I sense (generate interrupt) over the overall acceleration ?Because in the datasheet it was mentioned that I can manipulate the interrupt between X, Y, Z high and low.But it'd be helpful for me if I can generate an interrupt based on...

abduuu by Associate II
  • 327 Views
  • 1 replies
  • 1 kudos

Resolved! What are the benefits of sensor hub

Parts i'm looking to connect * STM32N6 - microcontroller * LSM6DSV320X -  Master Sensor IMU * LIS2MDL - On sensor hub Magnetometer     Question - is there any benefit to connecting the IMU master sensor to the LIS2MDL on the sensor hub vs connecting ...

LSM6DSV16X does not generate INT1 interrupt.

Hello.I am using an STM32H562VI board with an LSM6DSV16X sensor,and when I read the whoami value, it reads as 71.I configured the register as follows to check the interrupt on INT1./* Enable Block Data Update */ lsm6dsv16x_block_data_update_set(&dev_...

LSM6DSV16X .jpg LSM6DSV32X.jpg
heesu by Associate
  • 613 Views
  • 2 replies
  • 0 kudos