cancel
Showing results for 
Search instead for 
Did you mean: 

LSM6DSLTR and ESP32 - one axis of gyro is not detecting

SatyajitS
Associate

 

I am currently working with the LSM6DSLTR IMU sensor, interfacing it with an ESP32-S3-WROOM-1-N8R2 using the I2C protocol. However, I have encountered an issue where one of the accelerometer axes is not providing any data.

Issue Observed:

  • The sensor initializes correctly, and two axes provide valid acceleration values.
  • However, one axis does not provide any readings or returns a constant value.
  • The gyroscope readings appear normal.
  • I have verified the I2C connections, sensor power supply, and tested multiple units, but the issue persists.
1 REPLY 1
Andrew Neil
Super User

Welcome to the forum.

Please see: How to write your question to maximize your chances to find a solution - in particular, How to insert source code.

Please show schematics.

Some good, clear photos of the setup may also help.

 


@SatyajitS wrote:

I have verified the I2C connections, sensor power supply, and tested multiple units, but the issue persists.


Have you used an oscilloscope to very the signals on the I2C lines in the analogue domain?

In particular, are your pullups sensible?

Have you used a logic analyser (or similar) to very the comms between your ESP32 and the LSM6DSLTR ?

 

PS:

It appears you're using Arduino, so have you tried this:

https://github.com/dycodex/LSM6DSL-Arduino

 

PPS:


@SatyajitS wrote:
  • one axis does not provide any readings or returns a constant value.

What is the "constant value"?

https://forum.arduino.cc/t/arduino-uno-i2c-data-reading-problem/1175549

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.