MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Sensortile.box. Won't stay connected to Bluetooth

Original title: "Trouble with Sensortile.box. Won't stay connected to Bluetooth. Firmware upgrade to V349 completed, but no example apps. Works once, after reflash, can run new app I created, but then stops. Ran upgrade procedure several times, same ...

SGold.6 by Associate II
  • 1381 Views
  • 0 replies
  • 0 kudos

Resolved! LIS3DH - Issue with using the DREADY interrupt

Hi,I've tried to configure the DREADY to INT1 and read the output registers. I believe I'm making some mistake in the configuration as I observed that I'm able to read the OUT registers when I using the polling method. I've tried using the ST MEMS C ...

GTS.1 by Associate III
  • 1728 Views
  • 2 replies
  • 0 kudos

we connected STM32F051 to ASM330 over SPI . The communication works only with Chip select line being toggled LOW as a GPIO line the SPI is not able to set Chip select Low . There is a 10K ohm Pull-Up resistor on the Chip Select Line . What is the suggeste

Hi ,We connected STM32F051 to ASM330 over SPI . The communication works only with Chip select line being toggled LOW as a GPIO line the SPI is not able to set Chip select Low . There is a 10K ohm Pull-Up resistor on the Chip Select Line . What is the...

ck.1 by Associate III
  • 1950 Views
  • 1 replies
  • 2 kudos

Resolved! ISM303DLC Library

Hi i am using ISM303DLC sensor could you please suggest me which library i have to integrate to get the Roll, Pitch and Heading.

Anil3 by Associate III
  • 2022 Views
  • 3 replies
  • 2 kudos

Is the LSM6DSL command set compatiple with LSM6DSM?

I have a custom PCB with a LSM6DSM accelerometer and it's being controlled with a nRF52 running Zephyr. The Zephyr RTOS sensor libraries only have LSM6DSL and LSM6DSO devicetrees. According to the initialzation functions it's communicating correctly,...

BKrug.1 by Associate II
  • 1418 Views
  • 1 replies
  • 0 kudos

Resolved! Conformal coating - LIS2DW12TR

Hi TeamWe are currently working on ST PN: LIS2DW12TR in our new project. Thus, I would like to check with ST whether this part is OK to be Conformal coated? The reason is, our PCB will need to be conformal coating after all the components are populat...