User Activity

IS STM32H750 TFBGA240 PIN TO PIN Compatible to replace with STM32H755 TFBGA240
Hi ,Is there any Schematic of ASM330 connections over SPI to STM micro-controller for our Reference design . Please share if there is any reference design of ASM330 connections over SPIThanks
Hi ,We connected STM32F051 to ASM330 over SPI .The communication works Chip select as a GPIO line the SPI is not able to correctly toggle the Chip select . There is a 10K ohm Pull-Up resistor on the Chip Select Line between STM and ASM . Is this corr...
Hi ,We connected STM32F051 to ASM330 over SPI . The communication works only with Chip select line being toggled LOW as a GPIO line the SPI is not able to set Chip select Low . There is a 10K ohm Pull-Up resistor on the Chip Select Line . What is the...
Hi ,We have SEGGER J-TRACEpro for CORTEX-M processors . https://shop-us.segger.com/product/j-trace-pro-cortex-m-8-18-00/ We want to take the Code Coverage report . We are using Ozone IDE and loading the .OUT file to the OZONE IDE .There are 2 cables ...
Kudos from