MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! lsm6dsv320x WHO_AM_i

We're looking to use the lsm6dsv320x in our product. I'm using this senser on the on the STEVAL-MKI247A adapter board for testing. We're currently in development using the adapter board with the Nordic nRF52840DK board. I'm having issues with getting...

Screenshot 2025-07-03 114225.png
fk by Associate II
  • 4334 Views
  • 19 replies
  • 8 kudos

Resolved! Inconsistent whoAMI address of LSM6dsv320x on eval kit mk 1251

I have bought a new eval board from semikart via aquatronics. The device mounted on dil 24 of mk1251 kit is lsm6dsv320. The whoamI address of the device is 0x73 but it was not coming when we integrate with nucleo board. So, I waited for eval kit IKS4...

rv_08 by Associate II
  • 684 Views
  • 2 replies
  • 1 kudos

Resolved! XYZ values from AIS2IH are inconsistent with actual values

Hi, Post-development testing of the acceleration sensor reveals that the collected XYZ axis values are inconsistent with the actual physical acceleration values, and one axis continuously outputs a value of 0.What is the specific corresponding relati...

snack by Associate II
  • 1317 Views
  • 13 replies
  • 4 kudos

Resolved! ASM330LHHX : RES pin

Hi What is the function of the RES pins on the ASM330LHHX?The datasheet indicates: “Connect to VDDIO or GND.”Is there a preferred connection?Can I add a 4.7 kΩ pull-up or pull-down resistor?BR