MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Is the LSM6DSL command set compatiple with LSM6DSM?

I have a custom PCB with a LSM6DSM accelerometer and it's being controlled with a nRF52 running Zephyr. The Zephyr RTOS sensor libraries only have LSM6DSL and LSM6DSO devicetrees. According to the initialzation functions it's communicating correctly,...

BKrug.1 by Associate II
  • 1218 Views
  • 1 replies
  • 0 kudos

Resolved! Conformal coating - LIS2DW12TR

Hi TeamWe are currently working on ST PN: LIS2DW12TR in our new project. Thus, I would like to check with ST whether this part is OK to be Conformal coated? The reason is, our PCB will need to be conformal coating after all the components are populat...

Resolved! SPI receive the same data every time (it's the register who_am_i)

Hi!I'm using the LaunchPad CC2642R1/CC2652R1 with the accelerometer LIS2DH and i tested the "who am i" (0x33) register to validate the protocol but when i tried read another register i had the same response that "who am i" (0x33) register. Could you ...

0693W00000Y8yEeQAJ.png
TVela.1 by Associate III
  • 1861 Views
  • 9 replies
  • 0 kudos

SensorTile Dev Kit Cradle CPU gets hot

I have recently purchased the SensorTile development kit.I installed/soldered a sensortile and I noticed the LED didnt come on.I then felt the CPU was getting very hot.I reinstalled another sensorTile and the very same thing happened.Note I was extre...

lbbaker by Associate
  • 952 Views
  • 2 replies
  • 0 kudos

Resolved! LSM6DSR to LSM6DSOX migration issue

We are migrating from LSM6DSR to LSM6DSOX. In LSM6DSR the nominal timestamp resolution used to be around 25 μs. And we used to get 52 samples/sec from the FIFO.However, in LSM6DSOX with a similar setting, we are getting a resolution of around 18 μs. ...

Sachin3 by Associate
  • 792 Views
  • 1 replies
  • 0 kudos

Resolved! Driver issue on Windows 11

Hello communityI'm having issues with the STEVAL - MKI109V3 board and the Unico GUI. There is no driver identified for the board. I've tried installing the driver for Windows 8, which gets identified but when I try to open Unico GUI, I get an error m...

BVilm.1 by Associate
  • 1869 Views
  • 1 replies
  • 0 kudos