MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Wrist tilt and "funny" data in FUNC_SRC2

Hi,I trying to get the wrist tilt working. I have used the example in AN5040 page 55.I using the simple example setup, nothing else is set. Write 20h to CTRL1_XLWrite 84h to CTRL10_CWrite 01h to DRDY_PULSE_CFGWhen reading the FUNC_SRC2 it always retu...

TStee.1 by Associate
  • 1251 Views
  • 1 replies
  • 0 kudos

How to continuously read LSM6DSRTR data under Linux iio?

I am using​ LSM6DSRTR, and the device-tree compatible is "st,lsm6dsr".I can see two iio device node under​/sys/bus/iio/devices/iio:device1 /sys/bus/iio/devices/iio:device2But when I try to read in a python loop, it gets really slow.​Anyway better to ...

WYang.9 by Associate
  • 1925 Views
  • 1 replies
  • 0 kudos

Utilizing STEVAL-MKSBOX1V1 for Angle/3D Orientation Estimation

Hi all,I am currently working with STEVAL-MKSBOX1V1 to estimate the angle and 3D orientation of a static device. As I am limited to using the capabilities of the lis2dw12 chip only, I am relying on the accelerometer to provide the forces in the XYZ p...

SPiy.1 by Associate
  • 1462 Views
  • 1 replies
  • 0 kudos

print PCB for LSM6DSO with STM32WB55

Hello,I am working on an IOT project where we use motion sensors. Our prototype works with STM32WB55 + iKS01A3. We would like now to go further and replace iKS01A3 with LSM6DSO and print the PCB to put "between" the STM32WB55 and LSM6DSO. I've read a...

TMign.1 by Associate
  • 1529 Views
  • 1 replies
  • 0 kudos

LSM6DSOX AHRS Yaw measurement not correct

Hi there!​We are using the LSM6DSOX in our product and doing sensor fusion using xioTechnologies/Fusion.​Our hardware is mass produced and we are using the LSM6DSOX sensor with no magnetometer using 52Hz ODR and 104Hz ODR. The change in ODR doesn't s...

0693W00000Y9rNqQAJ.png
ladislas by Associate II
  • 1935 Views
  • 1 replies
  • 0 kudos