MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Is accelerometer drift in the LIS3DSH normal behavior?

I have an LIS3DSH securely mounted to a stationary object away from any vibration. Over the course of two and a half days, I've found the readings slowly change in value. I've tried this with multiple accelerometers (all LIS3DSH) and they always sh...

0690X00000ArfS2QAJ.png 0690X00000ArfS7QAJ.png 0690X00000ArfSCQAZ.png

Resolved! Re: X-nucleo-iks01a3's SPIs?

1. Are SPI_MISO/MOSI/CK/CS connected to STM32 MCU on the board? Logic Level 1.8V?2. Are SPI_MISO/MOSI/CK/CS_O for external connections on the board? Logic Level Vio?3. Are there a dedicated shunt for Vio connecting to 3.3V on the board?4.If a 3.3V lo...

QShan.1 by Associate II
  • 1431 Views
  • 1 replies
  • 0 kudos

Resolved! LSM6DSV - gyroscope bias

Hello ST community. I'm currently working with a LSM6DSV in a drone application. I would like to known if there is a suggested way to cancel the gyroscope bias value?

Resolved! ST BLE SENSOR APP MICROPHONE

Hello could someone explain me for the FFT LINE COMPARE that is in the ST BLE SENSOR APP for the sensortile.box what are the parameters that appear to edit? and also for the FFT COMPARE, which I understand that it will be the same and the "Name file ...

SAbba.1 by Associate III
  • 3686 Views
  • 2 replies
  • 0 kudos

Query about LSM6DSR read/write address on I2c interface

I am using LSM6DSR on I2c interface. As per datasheet when the SDO/SAO pin of the sensor is connected to ground the read/write address should be D5H/D4H but currently the read/write address is D7H/D6H. Can you please explain the reason for this? Has ...

RWasw.1 by Associate II
  • 3994 Views
  • 5 replies
  • 0 kudos

Resolved! LSM303AGR Temperature measurement??

Can anyone confirm if temperature measurement is functional on the LSM303AGR? I have everything else up and working just fine with measurements over several weeks, but temperature just return 0x00 for Hi and Lo byte. This is the third generation LSM3...

HFuxe.1 by Associate II
  • 3472 Views
  • 5 replies
  • 0 kudos

LIS2DTW12 FIFO modifying buffer size in continuous-to-FIFO mode

Hi,Is it possible to modify the amount of values that are written in the FIFO buffer after a trigger event has occurred in continuous-to-FIFO mode? Currently the device collects values in the FIFO buffer in continuous mode until a trigger event happe...

HNybl.1 by Associate
  • 1435 Views
  • 1 replies
  • 0 kudos