cancel
Showing results for 
Search instead for 
Did you mean: 

how can i change the STEVAL-MKI109V3 VDDIO to 3.3 V or get the INT1_up or INT2_up signals with an 3.3V Level?

BSeeg
Associate II
 
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Peter BENSCH
ST Employee

Welcome, @BSeeg​, to the community!

you can use the command *setvddio3.3 to set VDDIO=3.3V. This and all other commands are listed in UM2116.

Hope that helps?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
BSeeg
Associate II

Hello Peter

Is there a way to send comands in the unico Gui?

I tested The UART Interface and only the command

"*list"

did somthing

the Command

"*setdbMKI195V1" to select the LSM6DSRX Sensor i use got an

"inf Adapter nor supported" response

The conds *setvddio3.3 or *setvdda3.3 changed nothing nor got an response.

best regards Bene