cancel
Showing results for 
Search instead for 
Did you mean: 

Can i use STEVAL-MKI208V1K standalone ?

bcryhun
Associate II

I have STEVAL-MKI208V1K but not its own compatible motherboard. I want to use IIS3DWB sensor. When i connec SDA, SCL, GND and VDD(for vdd i have tried 3v3 and 5v), HAL_OK said HAL_ERROR. Is this STEVAL-MKI208V1K can be used standalone or no?

Thanks for helping

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Peter BENSCH
ST Employee

The STEVAL-MKI208V1K is just an adapter board with a sensor that makes the pins accessible via connectors. Of course, you can also use it stand-alone. However, the included IIS3DWB will almost certainly be destroyed by 5V supply voltage. When trying again, please do not forget the pull-ups on the I2C lines.

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.