MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SensorTile.box PRO project in STM32CubeIDE from scratch

  Hello. I would like to make a new project for the "SensorTile.box PRO" board using STM32CubeIDE. It appears that the board is not available. (In the image below, you can see that I have filtered on "box" and only the non-pro SensorTile.box device s...

stuart_rubin_ns_0-1699030180133.png

STEVAL-MK141V2 (HTS221) temp/RH sensor

Hi, I got the reference board of STEVAL-MKI141V2 that has HTS221 temperature and humidity sensor.#1I read out the calibration registers by the manual of https://www.st.com/resource/en/technical_note/tn1218-interpreting-humidity-and-temperature-readin...

Take4az by Associate
  • 1299 Views
  • 1 replies
  • 0 kudos

Unable to read registers from ISM330IS

Hello, I am trying to get a ISM330IS IMU working. I have ordered a development kit from Mouser / ST Micro with the following board number https://www.mouser.in/ProductDetail/STMicroelectronics/STEVAL-MKI230KA?qs=amGC7iS6iy%252B%252BWAEBNHSnWw%3D%3D (...

sa32953_0-1698726755935.png sa32953_1-1698726776353.png sa32953_2-1698726776150.png
sa32953 by Associate
  • 1188 Views
  • 1 replies
  • 0 kudos

How can I validate data rate of my sensors

Hello I'm trying to characterize LSM6DSO32X sensors on MKI221V1 using MKI109V3 evaluation board, It is crucial that I can see the output rate for my analysis.Unfortunately Unico GUI software doesn't seem to have an option to record the sensors with d...

Lev_G by Associate
  • 1393 Views
  • 1 replies
  • 0 kudos

Resolved! I3G4250 Not Updating Data At The Right Rate

I am using a I3G4250 on a custom PCB over I2C. When you first take data from it on restart it works but then after less than a second, it stops getting new data. It receives data exactly 25 times before stopping and sometimes receives about the same ...

Shock Survivability

What does "shock survivability" of a module mean ? Does it imply that the module reading with not change when the module exceeds the threshold value or will exceeding the limit kill the module ? For an application of +-25g , which IMU and pressure se...

H3LIS331DL

Hi,I readed the default value of the identification register in H3LIS331DL by SPI mode and it responded with 0x32h as per the data sheet,but while reading the STATUS REG default value it responded with 0xFFh instead of 0x00h. How it's possible one re...

Gokulraj by Associate II
  • 2086 Views
  • 2 replies
  • 0 kudos

Cannot open UNICO-GUI pkg on MacOS Ventura

When trying to download either Unico-GUI 9.14.6 or 9.13.0 I keep getting the error below. Any idea how to solve that on MacOS Ventura? I have already tried opening the pkg with control+right click, etc. with no success.  

andfer by Associate
  • 3872 Views
  • 2 replies
  • 3 kudos