MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to get 6DOF from STVAL-MKBOXPRO

Hi all,                               Can we get 6DOF(Acc + Gyro only) quaternion (Game Rotation Vector) data from STVAL-MKBOXPRO?. Is there any example available? kindly share the link.

Daya by Associate II
  • 1235 Views
  • 1 replies
  • 0 kudos

Resolved! Lenses for STHS34PF80 IR Sensor

Hello,We are currently in the process of developing a device that contains the STHS34PF80 IR sensor. After study of the datasheet and conducting our own tests, we have found that the sensor reliably detects a person within a 4-meter range. However, f...

KD2 by Associate II
  • 1955 Views
  • 1 replies
  • 0 kudos

The STTS22 temperature sensor gives me back 0 °C

Hello everyone,after some time that I use the sensor, it gives me back a temperature value of 0 °C.I'm using a library taken from github that I adapted to work with the STM32F407 microcontroller (can't post the link).The sensor works well but sometim...

SSerg.4 by Associate III
  • 2282 Views
  • 3 replies
  • 0 kudos

Why doesn't the gyro value come out

Hi,I am using the LSM6DSO32X(in STEVAL-MKI197V1) sensor on the STEVAL-MKI109V3 board.There is no external sensor.I see and follow the Datasheet, but the Gyro Data does not come out and the external sensor value comes out.I used Easy Configuration in ...

sygo_0-1701306155478.png
sygo by Associate II
  • 2436 Views
  • 4 replies
  • 0 kudos

Resolved! Issue with HTS221TR Sensor in the Presence of Product Projections

Hello everyone,I am an engineer at an EMS, and one of our clients has reported an issue related to the use of the HTS221TR sensor. Our client has observed that some of their boards, on which this sensor is mounted, have been exposed to projections of...

AxelH by Associate
  • 1532 Views
  • 2 replies
  • 1 kudos

LSM6DSO Sample Rate

Hello,I would like to increase the sample rate of a SparkFun LSM6DSO which is controlled by the ESP32 Thing Plus C microcontroller (I am using the Arduino IDE and said libraries).I tried using the function LSM6DSO::setAccelDataRate() and LSM6DSO::set...

ItaiS by Associate
  • 1570 Views
  • 1 replies
  • 0 kudos

Resolved! IMU sensor

Hi all, Is there any difference between LSM6DSV16x and LSM6DSV16xTR except the packaging?Thanks in advance.

Daya by Associate II
  • 7322 Views
  • 5 replies
  • 1 kudos