MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LSM6DSO FSM Testing

I want to do some testing and experimenting with the FSM features of the LSM6DSO. I have MEMS Studio downloaded, and I also downloaded the X-CUBE-MEMS1 expansion software package. I see on the documentation for X-CUBE-MEMS1 that the NUCLEO-L476RG was...

j_yunker by Associate
  • 520 Views
  • 1 replies
  • 0 kudos

Filltering on CCA02M2

Hey ST Community,I'm currently trying out the CCA02M2 MEMS microphone board on a NUCLEO-L476RG, using firmware compiled from X-CUBE-MEMSMIC1.The microphones work, but the signal seems to have some heavy filtering. For example:If I record with Audacit...

KRT by Associate
  • 416 Views
  • 0 replies
  • 0 kudos

How to get calibration level for IMU sensor and magnetometer

After soldering process, IMU sensor and magnetometer need to do calibration after power on, such as flip axis, 8 shaped pattern, or real-time calibration.For ST sensor such as LSM6DSV and LIS2MDL, I want to know how to confirm whether sensor has been...

Yansu by Associate III
  • 2336 Views
  • 4 replies
  • 0 kudos

Actual Detection Range and FOV of STHS34PF80?

Hello everyone,I’ve been working with the STHS34PF80 sensor and would appreciate some insights regarding its detection range and field of view (FOV). In my tests, I’ve observed that the sensor detects presence effectively up to a range of about 1 met...

mobaid by Associate II
  • 992 Views
  • 3 replies
  • 0 kudos

STHS34PF80

I am using the STHS34PF80 sensor (SparkFun Presence Sensor - STHS34PF80) with an ESP32 in my ceiling fan to automatically turn the fan ON and OFF based on human presence and motion. However, the sensor is providing continuously varying output values ...

Compatibility STEVAL-MKI227KA Arduino Mirco

Hello,I'm working on an IMU project. I need to measure pitch/roll/yaw rotation in quaternions.For my first test, I am using a STEVAL-MKI227KA connected to an Arduino micro, which already allows me to extract the quaternions.I send the data via I²C.My...

BapDBD by Associate
  • 304 Views
  • 0 replies
  • 0 kudos

LSM6DSO Migration from LSM6DSM

Hi Everyone,I'm currently migrating from LSM6DSM to LSM6DSO in my application and facing some issues with accelerometer accuracy in stable conditions.System Overview:MCU: STM32L4Sensor Interface: SPI (3-wire)Purpose: Reading raw accelerometer and gyr...

rshar21_0-1752843355517.png rshar21_1-1752843410485.png
rshar.21 by Associate II
  • 332 Views
  • 5 replies
  • 0 kudos