cancel
Showing results for 
Search instead for 
Did you mean: 

LSM6DSO FSM Testing

j_yunker
Associate

I want to do some testing and experimenting with the FSM features of the LSM6DSO. I have MEMS Studio downloaded, and I also downloaded the X-CUBE-MEMS1 expansion software package. I see on the documentation for X-CUBE-MEMS1 that the NUCLEO-L476RG was replaced with the NUCLEO-U575ZI-Q in November 2022. I also found X-CUBE-MEMS1-V4, but on the page, I cannot find a download link. I was wondering if someone could provide me the firmware for my setup, or some guidance on how I can get it working with MEMS Studio, so that I can play around with the FSM on the LSM6DSO.

1 REPLY 1
Peter BENSCH
ST Employee

Welcome @j_yunker, to the community!

this question is currently being processed via the Online Support (OLS) ticket # 00241517.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.