MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! IKS4A1 eCompass application with Unicleo-GUI

Hello, I am trying to test the e-compass application with the IKS4A1 connected to a Nucleo-F446 and Unicleo-GUI. The firmware of the Nucleo F446 was produced from Cube-MX following the "Getting started with the STMicroelectronics X-CUBE-MEMS1 softwar...

MRaff1_0-1706620923031.png
MRaff.1 by Associate III
  • 2342 Views
  • 2 replies
  • 1 kudos

LSM6DSM - Inquiry regarding 12-sec periodic noise

I have been experiencing a peculiar issue with the LSM6DSM sensor, where noise occurs at a 12-second interval. This phenomenon is consistent across multiple units and locations. Notably, the noise seems to affect only the Z-axis.Settings: with the AC...

Resolved! How to effectively use lis2dw12 to detect motionless event ?

Hi All,I need a mechanism to detect motionless for 10s to make device enter power saving mode.For lis2dh12, I can use HPF with low x,y,z threshold and duration to detect an event that motionless for 10s.However I need more low power accelerometer lis...

SLin.11 by Associate III
  • 4853 Views
  • 6 replies
  • 0 kudos

Resolved! LIS2DW12 FIFO overflows upon wake-up by interrupt

GreetingsI have configured  the LIS2DW12, via SPI,  to sample and store samples, given the FIFO (configured in continuous mode) on a wakeup interrupt to INT1. The sensor, given its current configuration is able to wake up and sample but there is a wo...

ZAIDS-S23 by Associate III
  • 2558 Views
  • 4 replies
  • 0 kudos

Resolved! ST tile box pro heading drift issue

Hi all,I am using ST tile box pro and logging IMU orientation data for my test. I did place that module in a robotic arm and then calibrate the accel sensor. I observed 20 degree drift in the  heading value  after the calibration .Before calibration ...

Accelerometer and gyroscope

Hello,I need to measure the tilt angles (along the x, y, z axis) of a flying device. What accelerometer can you recommend produced by STM? Will one accelerometer be enough? Or do you still need a gyroscope to complete the task?

ASM330LHB on STEVAL-MKI236A difficulty connecting via I2C

I am trying to connect the IMU sensor that is onboard the STEVAL_MKI236AA evaluation board. I am currently trying to connect that board to BeagleBone AI-64 or a basic Arduino via I2C and was able to detect an I2C device as 0x6A and 0x6B as the board ...

PXL_20240127_174704392.jpg

Resolved! Unicleo-GUI does not connect

Hello,    I am trying to test the compass of the IKS4A1 board with a Nucleo F446 board. I followed line by line the instructions provided in the "Getting started with the STMicroelectronics X-CUBE-MEMS1 software package for STM32CubeMX". My cube proj...

MRaff1_0-1706287076093.png
MRaff.1 by Associate III
  • 2824 Views
  • 3 replies
  • 1 kudos

LSM303AGR X-CUBE-MEMS1

Hello,    I have a custom board with a STM32F373 and a LSM303AGR MEMS device.I made a Cube-MX project in which I included the corresponding x-cube-mems1 software pack with an eCompass application.The project compiles and runs. I see from the firmware...

MRaff.1 by Associate III
  • 1724 Views
  • 2 replies
  • 0 kudos