MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Response time of LPS sensor

Hello, "1/ODR (1 à 200 HZ)" is it the response time of the sensor ?Thank you 

ljm by Associate III
  • 1436 Views
  • 2 replies
  • 1 kudos

AIS2IH VDD_IO Supply Current

Hello,What is the supply current into the VDD_IO pin on the AIS2IH? The VDD supply current requirements are explained in detail, but I do not see any note on the current into the VDD_IO pin.Best regards

Resolved! LSM6DSO Single + Double tap (LIR bit = 1) => Only single tap interrupt.

According to AN5192 (last paragraph of page 50) if LIR is enabled (0x56:0x4F)  and SINGLE_DOUBLE_TAP is set (0x5B:0x80) "latched mode is applied to the double-tap interrupt signal only".But I only read single tap in TAP_SRC (0x1C:0x20) during ISR.As ...

F_G by Associate
  • 1952 Views
  • 3 replies
  • 0 kudos

Resolved! St-mems-android-linux-sensors-hal Snapdragon ADSP compatibility

Hi,From the following repo https://github.com/STMicroelectronics/st-mems-android-linux-sensors-hal/tree/masterI would like to know if the driver it's compatible with an Android environment under snapdragon where all the sensors part is managed under ...

DevM by Associate II
  • 2479 Views
  • 2 replies
  • 0 kudos

[iis3dwb] Read sensor data without loss.

Hi, I want to receive data coming from the sensor without loss.For the testing, sampling rate is set to 32Hz.26667(ODR) / 800 = 32hzif set like this, 32 data per second will be accumulated in the buffer.and CNT_BDR_THR was set to 100.also, FIFO_MODE ...

HKim23_0-1710154197476.png
HKim.23 by Associate III
  • 2908 Views
  • 4 replies
  • 1 kudos

Resolved! [IIS3DWB] Sampling rate set to 2K band.

Hi,I want to set the raw data to around 2k bandwidth and receive all data through FIFO.From what I understand, to set it to 2k bandwidth-Bandwidth ODR/4 = 2.6kHz, HPCF_XL = 0, LPF2_XL_EN =1-FIFO_CTRL3 BDR_XL = 0b1010 ( 26667Hz ) And at this time, if ...

HKim.23 by Associate III
  • 1829 Views
  • 2 replies
  • 0 kudos

Resolved! setup LIS2DUX12TR for motion detection

Dear all,I want to set LIS2DUX12TR to detect if there is a motion of the board, like a theft detector.The board is battery powered, so, I was thought to use INT1 pin to wake my PIC18LF26K22 uC to send some data.For me, is for time when I interact wit...

costi002 by Associate
  • 2264 Views
  • 2 replies
  • 0 kudos

Using multiple interrupts on 1 interrupt pin - LIS2DW12

GreetingsI am currently using the LIS2DW12 accelerometer, in continuous-to-fifo mode, with the wake-up interrupt configured to INT1, and the DIFF5 interrupt configured to INT2. All works well, as I'm able to read the FIFO contents when the FIFO is fu...

ZAIDS-S23 by Associate III
  • 4221 Views
  • 1 replies
  • 0 kudos