MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LPS25HBTR_Recommended Land pattern

Hi Team,In our design we planned to use this part LPS25HBTR (Pressure sensor). As per Datasheet Recommended land pattern is not available. Could you please share PCB land pattern for this part LPS25HBTR. Thanks & Regards,Karthikeyan

LIS2MDL - impact to ODR When Set_FREQ = 1

Hi  Can someone clarify how long it takes for the sensor to temporarily stop reading, execute the SET pulse, and begin conversion when Set_FREQ is set to 1 in CFG_REG_B (61h) while in continuous conversion mode? I noticed that this setting randomly c...

Indi by Associate
  • 1193 Views
  • 1 replies
  • 0 kudos

LIS2MDL OSR rate

HelloDoes anyone know the signal Oversampling Rate/s?I'm working for a Medtech company developing a novel device and we are thinking of using the LIS2MDL for our analysis. The data from the sensor will be analysed using different signal processing te...

Indi by Associate
  • 1338 Views
  • 1 replies
  • 0 kudos

Resolved! LSM6DSO(X) FSM Threshold Confusion

Hi all,This should be a question with a simple answer, but for some reason, I cannot find clarification. I am trying to use the Finite State Machine in the LSM6DSOX, and I have come across these examples below in this application note:I'm confused on...

Screenshot 2024-03-15 095604.png
jspear by Associate II
  • 1351 Views
  • 1 replies
  • 1 kudos

Resolved! Audio functionality on LSM6DSV16B accelerometer

HeyLSM6DSV16B is sold as an accelerometer unit that can be used to record vibrations as an audio signal. The datasheet mentions that this audio signal can be placed on the TDM interface, but I doesn't really say how.Does anyone have experience with t...

EYako.1 by Associate III
  • 4254 Views
  • 7 replies
  • 4 kudos

Getting started with STEVAL-BCN002V1B, temperature via bluetooth

Hi everyone, some of my initial issues have been solved while one is still remaining. Most Bluetooth 5 devices cant connect to the Bluetile sensor node. I have to use the programmer board with the sensor node on it connected via USB to establish a bl...

Bluetile.png
Sonntag by Associate II
  • 1624 Views
  • 1 replies
  • 0 kudos

LIS2MDL number of samples in low power mode Vs high resolution mode

Hi,I'm looking for the information about the number of sensor ADC samples per output data, in low power mode Vs. the high resolution mode.I found the following description in AN5069:"The difference distinguishing the two modes is in the number of sam...

dagan by Associate II
  • 1763 Views
  • 3 replies
  • 0 kudos