MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIS2DH12 acceleration data not changing

Dear All, I am using the LIS2DH12 accelerometer that is incorporated within a Decawave DWM1001-DEV board. I am attempting to write a C program using the dwm.h library functions to display the acceleration values for the X, Y and Z axes via I2C consta...

GChan_02_0-1711436593131.png GChan_02_1-1711437056735.png GChan_02_2-1711437118612.png
GChan_02 by Associate
  • 2096 Views
  • 1 replies
  • 0 kudos

Query regarding IMU sensor for Golf Swing Analyses

Posted on October 23, 2015 at 08:33I am in search of 6 or 9 axis IMU mems sensor for golf swing analyses device. The device would be somewhat like  http://3bayslife.com/zone-1/ Should I go for 6 axis DOF or 9 axis DOF? Low power operation is must. A...

rahul23 by Associate
  • 2214 Views
  • 3 replies
  • 0 kudos

Resolved! Negative sign for TMOTION and TPRESENCE on STHS34PF80

I am using the STHS34PF80 sensor to detect motion and presence. When I read the raw value of TMOTION and TPRESENCE I get both positive and negative numbers. What does the negative sign indicate here? Thanks

jkutteh by Associate II
  • 5723 Views
  • 10 replies
  • 1 kudos

MotionVC Lib Implementation & Data Drifting

Hi all, I am trying to use the MotionVC library functions to return my vertical speed and calibrated speed, however I have encountered two unknowns: the internal timing or buffer processing of the MotionVC_Update() function and why the calibrated alt...

LIS3DH using I2C HAL - Not reading acceleration data

Hi everyone,Based on the drivers from ST GitHub, I developed my own one, but I can't understand why it's not working. I can communicate with the accelerometer and I can read the registers, but I don't know why i am having troubles to read the acceler...

LaraCS by Associate II
  • 2625 Views
  • 4 replies
  • 1 kudos

ASM330LHHX stops transmitting after some time.

I am using Nucleo F767ZI with SPI interface to ASM330LHHX sensor. I am using example code from https://github.com/STMicroelectronics/STMems_Standard_C_drivers/blob/master/asm330lhhx_STdC/examples/asm330lhhx_read_data_polling.cAfter a couple of second...

MAnto.2 by Associate III
  • 1653 Views
  • 2 replies
  • 2 kudos

Resolved! L3gd20 sensor on stm32f411e-discovery

I am practicing reading L3GD20 data built into the stm32f411e-discovery kit. I use SPI1 to communicate with L3GD20. I watched on YouTube, they have instructions on how to use the void function HAL_GPIO_EXTI_Callback. I cannot call the void HAL_GPIO_E...

image.png image.png image.png image.png

LSM303AGR temperature measurement

Hi everybody,I'm using a LSM303AGR and I got some difficulties to read the temperature.My I2c functions, because I can read "who am I" registers, and I tried to write then to read some registers. I did the following steps :     LSM303_IO_Write_one_by...

LSM303.png
fab04 by Senior
  • 1364 Views
  • 1 replies
  • 0 kudos