cancel
Showing results for 
Search instead for 
Did you mean: 

LIS2MDL - impact to ODR When Set_FREQ = 1

Indi
Associate

Hi 

 

Can someone clarify how long it takes for the sensor to temporarily stop reading, execute the SET pulse, and begin conversion when Set_FREQ is set to 1 in CFG_REG_B (61h) while in continuous conversion mode?

 

I noticed that this setting randomly changes my ODR rate. 

 

Thank you.

 

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Federica Bossi
ST Employee

Hi @Indi ,

Which difference in the ODR rate did you notice?

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.