MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ism330dhcx - 6dof position + orientation estimation algorithm

im using the ism330dhcx in an application where POSE (position + orientation) estimation are required.the accelerometer and gyroscope data are written to an SD card @ 100Hz and will be post processed to keep things simple, however, if anyone has a re...

mvs1970 by Associate II
  • 2824 Views
  • 3 replies
  • 0 kudos

Problem with MS5611 Barometer Pressure Reading

Posted on November 28, 2017 at 14:27Hi all! I am trying to read temperature and pressure values (then, convert pressure to altitude) from MS5611 barometer using I2C interface with STM32F4. So far, I managed to read both temperature and pressure valu...

lsm6dsox sensor

lsm6dsox sensor generates significant motion interrupt when a change in user location is detected. It generates an interrupt when the difference between the number of steps counted from its initialization/reset is higher than 10 steps. So it uses ste...

rena by Associate II
  • 2269 Views
  • 3 replies
  • 0 kudos

lsm6dso inactivity detection

What is the maximum time-limit in minutes that can be set in the register LSM6DSO_WAKE_UP_DUR, for inactivity detection. I want to rise an interrupt after 20minutes. How is it possible? 

Varsha by Associate III
  • 2972 Views
  • 4 replies
  • 1 kudos

Resolved! LPSS22DF accuracy between -15°C and 60°C

HiI'm currently using your LPS22DFmodule to measure pressure and I saw in the datasheet that the temperature accuracy is  ±1.5 °C (T = 0 to 80°C). My working range is between -15°C and 60°C. Could you please give me the accuracy of this sensor in the...

ljm by Associate III
  • 8220 Views
  • 14 replies
  • 1 kudos

STEVAL-STWINKT1B - Battery Operation with 3.7V

Hi everyone,I'm working with the STEVAL-STWINKT1B and have a question about powering it with a 3.7V battery. The board uses the STBC02 PMIC, which operates between 4.5V and 5.4V according to its datasheet.The datasheet suggests the STBC02 charges a b...

dhruvit by Associate II
  • 1444 Views
  • 0 replies
  • 0 kudos

Resolved! ST MEMS studio - STEVAL STWINBX1 - Connection error

I'm having problems to be able to establish the connection between STEVAL STWINBX1 and ST MEMS Studio software, with either of the two available ways (BLE or Serial port). In the first case, mainly the board won't be shown to select. In case it does,...

jvf_13 by Associate
  • 2871 Views
  • 2 replies
  • 1 kudos

[STHS34PF80] TPRESENCE and TMOTION units

I searched all available documentation, community and haven't found answer.AN5983 says nothing about motion and presence units.Code base (https://github.com/STMicroelectronics/sths34pf80-pid) and datasheet also say nothing about motion and presence u...

MarcinJ by Associate
  • 1378 Views
  • 1 replies
  • 0 kudos

LSM303AGR magnetometer will not pass self test

Hello,I have been battling with getting an LSM303AGR to pass the self test. The accelerometer is passing the self test and the values look reasonable (Z-axis ~1g), but the magnetometer will not pass. I have 2 STEVAL-MKI172V1 boards, both are showing ...

ocean_rse by Associate II
  • 3847 Views
  • 4 replies
  • 0 kudos