MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIS2DH12 Z-axis value is reported with the opposite sign

Hi,I've been working with the LIS2DH12 sensor for quite some time, primarily utilizing the X and Y axes without any issues. However, for a new project, I also need to incorporate the Z-axis. I've noticed that while the acceleration values reported ar...

LJim1_0-1712836405290.png
LJimé.1 by Associate III
  • 2341 Views
  • 2 replies
  • 0 kudos

Resolved! Question about LSM303AGR_ACC_SENSITIVITY_2G definition in lsm303agr.h

Hello STM32 community,I've been examining the lsm303agr.h file from STMicroelectronics for the LSM303AGR accelerometer, and I came across something puzzling in line 197. In the code, it defines LSM303AGR_ACC_SENSITIVITY_2G as ((uint8_t)1), but accord...

Duc by Senior
  • 1967 Views
  • 2 replies
  • 0 kudos

About IIS3DWB FIFO watermark setting

I modified this IIS3DWB example to use IIS3DWB on my nRF board.This example set the size of watermark as 256,and in the while loop, the data will be retrieved when FIFO_WTM_IA is triggered. In my program, it seems that I can get the correct accel dat...

chenjy96 by Associate
  • 1450 Views
  • 1 replies
  • 0 kudos

MotionAC doesn't seem to be working.

Hi,I am trying to perform a 6-point tumble calibration for my LSM9DS1 accelerometer. The returned output data from the MotionAC_Update is always as follows:The "is_calibrated" parameter is always 0, indicating the accelerometer is not calibrated.The ...

0693W00000APNhrQAH.jpg
PMach.1 by Senior
  • 3726 Views
  • 5 replies
  • 0 kudos

Resolved! LIS2DS12TR Marking

We have received LIS2DS12TR, but we cannot identify the Marking of the Part.On the part there is a QR-Code and a "G". Could you please confirm that this is LIS2DS12TR and what the QR Code is standing for. Thank you in advance

Resolved! LSM6DSL gyroscope high-pass filter reset

Hi all,I have a question regarding the LSM6DSL's gyroscope high-pass filter configuration.For LSM6DS3, there is an option to reset the high-pass with HP_G_RST = 1. This way, the DC component of the angular velocity is immediately removed, c.f. https:...

flaufer by Associate II
  • 2122 Views
  • 2 replies
  • 1 kudos

Resolved! LIS344LH accelererometer

Good morning,I work actualy with the LIS344LH accelererometer and I was informed it will not be available anymore.Do you know any other devices that would substituate it ? I need it for measuring the movement of a tuning fork with a resonnance freque...

fru999 by Associate III
  • 1406 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.