HiIn our design, we incorporated the IMS T225-F20E component. This part necessitates a clock with a frequency of 5 MHz. According to note 3 in the attached image, crystal oscillators with a 200 ppm (parts per million) tolerance can be employed. Howev...
Hi,We are using ASM330LHHTR in our design. Could you please share the TARIC code details for this particular component? Additionally, could you provide the information on the End-of-Life status of this part?Regards,Sowmiya
Hi,Greetings!We are planning to use ASM330LHHTR in our design. As per the datasheet of Gyro sensor chip, it is recommended to have a decoupling capacitor of 0.1uF+10uF (Aluminum). Since we don't have enough space in our board to accommodate the Alumi...
Hi ,The part L3GD20HTR has mechanical drawing at page 49-50 with 16 pins as per the datasheet, but in the document TN1198 ,PCB design guidelines has 6 pads only with no pin numbering. Do we need to create 16 pads with the available pad dimensions in ...