Skip to main content
Associate
December 21, 2023
Question

Temperature Conversion - from the LIS3DH sensor raw value

  • December 21, 2023
  • 4 replies
  • 1914 views

Hello All,

Need to read the values from the embedded Temperature Sensor in LIS3DH via I2C communication 

I had made the following configurations as mentioned in the datasheet,

1. CTRL_REG4(0x23) = 0X80

2. TEMP_CFG_REF (1Fh) = 0XC0

3. Trying read the temperature value from the following register OUT_ADC_3_L(0x0C) and OUT_ADC_3_H(0x0D).

     - Getting the value from the OUT_ADC_3_H(0x0D) as 8. If I expose heat near to the chip the value is increasing. 

How to convert this(8) value to temperature?

Kindly assist me to get the conversation formula. Here the Vdd supply = 3.3V.

 

Thanks in Advance.

 

Regards,

Surya S 

  

This topic has been closed for replies.

4 replies

Federica Bossi
ST Technical Moderator
December 21, 2023

Hi @Surya S ,

As reported in Table 5 of the datasheet, the temperature sensor output change vs temperature: 1 digit/degree of Celsius.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Surya SAuthor
Associate
December 26, 2023

@Federica Bossi ,

 

Thank you for the update.

 

Here the thing is the unit we kept the unit under room temperature 25°C and the value read from the register OUT_ADC_3_H(0x0D) is 7. How can equate this  8 to 25°C? Attached image is for your reference.

 

SuryaS_0-1703582396726.png

Thanks In Advance.

 

Tesla DeLorean
Guru
December 26, 2023

You should be able to read both the low and high byte in a singular 2 byte read operation. What's that number pair?

Post code section using the ... </> tool in the post edit window, not as a bitmap

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..