MEMS (sensors)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How do you install PDM library ?

I struggle to use PDM Filter library.This is the message error I get : What I have done so far are : - in project properties, C/C++ general, Paths and syombols, in "Includes" I added the path to pdm2pcm_glo.h ; in "Library Paths" I added the path to ...

0693W00000KbhBQQAZ.png 0693W00000KbhEyQAJ.png
EEnco.1 by Associate III
  • 1891 Views
  • 10 replies
  • 1 kudos

6 pdm microphones with MEMSMIC1 example

Hello, I am currently running the MEMSMIC1 audio streaming example via usb with 4 channels and it works fine, but Because i am using the nucleo-wb55 board that has a pdm interface supporting up to 3 microphone pairs I want to use as many microphones ...

lsm6dso remove g from acceleration

I would like to eliminate the influence of the gravitational field g from the measurement of accelerationI tried with a high pass filter. Is this the only solution?The problem is that the sensor evolves in space with orientations that vary over time....

chan by Associate
  • 390 Views
  • 1 replies
  • 0 kudos

H3LIS331DL

Hi,I readed the default value of the identification register in H3LIS331DL by SPI mode and it responded with 0x32h as per the data sheet,but while reading the STATUS REG default value it responded with 0xFFh instead of 0x00h. How it's possible one re...

Gokulraj by Associate II
  • 532 Views
  • 2 replies
  • 0 kudos

Resolved! (SOLVED) SPI communication problem with sensors

I'm using STEVAL-STWINKT1 (MCU STM32L4R9ZIJ6) and I'm trying to communicate with the motion sensors (ISM330DHCX, IIS3DWB, IIS2DH) by SPI3 interface (polling). I wrote a code very similar to that one present in the "Serial_DataLog" project, using HALs...

irene by Associate II
  • 1633 Views
  • 7 replies
  • 0 kudos