Skip to main content
Visitor II
November 11, 2023
Question

lsm6dso remove g from acceleration

  • November 11, 2023
  • 1 reply
  • 1130 views
I would like to eliminate the influence of the gravitational field g from the measurement of acceleration
I tried with a high pass filter. Is this the only solution?
The problem is that the sensor evolves in space with orientations that vary over time. If the variations in acceleration evolve at the same rate as the orientation of the sensor, the low pass filter eliminates g but also eliminates the acceleration. how to do ? Thank you for your help !
This topic has been closed for replies.

1 reply

Federica Bossi
ST Technical Moderator
November 17, 2023

Hi @chan ,

I confirm you that a High Pass Filter is the only possible solution.

Otherwise you can implement a sensor fusion using the gyroscope, you can look at our Motion FX library here, or at our IMU with embedded sensor fusion, such as the LSM6DSV.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.