My configuration is when button is pressed start advertising and stop advertising after 100ms. When the button is pressed a few times device gets hung and continuously advertises.When I tried debugging following is the traces I didn't understand thi...
Hi, I want to develop a basic Zigbee end device.After having successfully programmed a STM32WB55 Nucleo with the example Zigbee_OnOff_Server_Distrib, I tried to use CubeIDE to setup from scratch my own device. I am unable to set CFG_DEBUG_TRACE, as i...
Hi,I am using STM32WB55CG6 custom board and configured as cliend and trying to connect with server(ESP32 configures as server).When a button is pressed i am connecting to server =============================================================void HAL_GP...
Hi Team,We are using the Flash Operations as part of Data saving in specific page. As part of that we are erasing the page and writing the new data. As Part of the Flash Erase operation, we are Entering into HardFault_Handler() function through the F...
I'm using the STM32WB55, with STM32CubeWB V1.14.1 & `stm32wb5x_BLE_Stack_full_fw.bin` V1.14.1.Looking in `app_debug.c`, I can configure `aGpioConfigList[]` and `aRfConfigList[]`, which allows for CPU2 to toggle a GPIO pin based on various events.I ca...
In the application BLE_OTA for STM32WB55 NUCLEO 64 board there is no Debug configuration. It is also mentioned in the project's readme.txt file that "Debug configuration of BLE_Ota CubeIDE project is not supported by current BLE_Ota application setti...
Hi, I want to configure the USART1 as TRACE in LORAWAN_AT_Slave project. I tried replaced LPUART with USART1 in the MDK-ARM but my project's TRACE not work. Any one know how to replace LPUART with USART1 ?
I'm developing my custom board using a STM32WB55VGY6TR microcontroller and I want to use the Nucleo-WB55 developer kit as a programmer for my custom circuit board.However, I cannot start debugging using STM32cubeIDE. The IDE said that failed to start...
Hi,My problem is that I have "no stm32 traget found" message when I try to connect to a board by SWD through a ST-Link/v2 (no board identified). On oscilloscope, when we look on SWDIO pin, a little event happens when initializing connection on stm32c...