User Activity

I am using the STM32G474 and have the following situation:I have configured a Timer to run continuously at 25 kHzThe Timer triggers the ADC to start a sequence of 6 conversions (i.e. 6 ADC channels)Upon completion of each ADC conversion, DMA transfer...
I'm using the STM32WB55, with STM32CubeWB V1.14.1 & `stm32wb5x_BLE_Stack_full_fw.bin` V1.14.1.Looking in `app_debug.c`, I can configure `aGpioConfigList[]` and `aRfConfigList[]`, which allows for CPU2 to toggle a GPIO pin based on various events.I ca...
I'm am looking to prototype an RFID system that involves communicating with a 'smart' passive TAG at a range of about 40cm. Which evaluation boards (reader and passive tag board) would be best suited for this application?I'm am looking to prototype a...
Kudos given to