User Activity

Hello,https://www.st.com/content/dam/OLM%20Email%20Marketing/2021/EMEA/Events/BlueNRG-LP/STBLEBlueNRGLPWebinarApril20V3.pdfIn page 9 of the above document STM is mentioning FFT - my question is - where can I find libraries for FFT, FIR etc. for Blue...
In the application BLE_OTA for STM32WB55 NUCLEO 64 board there is no Debug configuration. It is also mentioned in the project's readme.txt file that "Debug configuration of BLE_Ota CubeIDE project is not supported by current BLE_Ota application setti...
As an example, the following code is provided, the timers are started and stopped in app_ble.c.I can run two of the three leds using two different timers and they work properly, but when I add the third one than the leds start working in an unexpecte...
I'm trying to run broadcasting mode on the base off BLE_P2PServer example and instead of aci_gap_set_discoverable in app_ble.c, in "Adv_Request" function, I'm trying to use the below function:  aci_gap_set_broadcast_mode( Min_Inter, Max_Inter, ADV_NO...
Kudos from