STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1393 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 549 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! STLinkUpgrade utility text is too small to read

The font size used for the GUI in the STLinkUpgrade utility so small it is virtually unreadable on the external 32" 4K monitor that I use with my laptop. The following shows the text size relative to code within the IDE:It's possible that this is as ...

CTapp1_0-1748251211537.png CTapp1_1-1748251544211.png
CTapp.1 by Senior III
  • 1156 Views
  • 3 replies
  • 0 kudos

Resolved! STM32CubeIDE 1.17.0 unable to programm STM32H730

Ther seems to be a problem in the STM32CubeIDE versione 1.17.0 when debugging / programming the STM32H730 chip.The Programmer returns: ST-LINK SN : 002800045553500F20393256 ST-LINK FW : V3J15M7B5S1 Board : STLINK-V3SET Voltage : 3.28V Err...

MHoll.2 by Senior III
  • 2035 Views
  • 4 replies
  • 0 kudos

Resolved! STM32H563: BANK SWAP

I am using NUCLEO-H563ZI and am trying to implement bank swap for firmware update. I am using YMODEM to update firmware. Initially when my code is being executed from BANK 1 and after writing the new firmware at BANK 2. The code execution starts from...

Resolved! Creating CMake project for STM32U5 divide memory

I'm using STM32CubeIDE 1.18.1 and when i create a new STM32 CMake Project for a STM32U5, the generated ld file contain only half the memory.For example here what is generated in STM32U575ZITXQ_FLASH.ld:MEMORY { RAM (xrw) : ORIGIN = 0x20040000, LENG...

nicolas by Senior II
  • 1761 Views
  • 4 replies
  • 2 kudos

FreeRTOS and USB givers Hard Fault in H743 MCU

  Dear Sirs I am having a problem using FreeRTOS and USB on H7 series MCU. The IDE gives “Hard Fault” when I debug the project. See image below.   The environments are : STM32CubeIDE:  Version: 1.14.0, Build: 19471_20231121_1200 (UTC) Target: NUCLEO...

RAbdu1542_1-1708960464673.jpeg

execute nested functions in RAM on STM32F746

Hello, I'm trying to get running own external loader for CubeMX compiled with CubeIDE.I have followed this internet source to set-up envirement but without success. Because the CubeMX plugin doesn't work I tried to debug RAM-execution without CubeMX....

Wlad777 by Associate II
  • 1198 Views
  • 2 replies
  • 0 kudos

Make SWO character output non-blocking?

Correct me if I'm wrong, but it seems that ITM_SendChar() is blocking on the character transmission. Has anyone attempted to compensate for this or do people just put up/move to a UART?At this point all I can think of is to implement a FIFO queue and...

Grant Bt by Senior II
  • 1292 Views
  • 4 replies
  • 3 kudos

Tooltips background text is black and text not visible

Hi,In STM32CubeIDE code editor when I go over a variable or function the tool tip window that opens and shows the declaration of variable or implementation of the function  - the window has a black (very dark background ) and text is also black and n...

Screenshot 2025-05-11 085913.jpg
CSand by Associate III
  • 1836 Views
  • 4 replies
  • 0 kudos