STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1393 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 549 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

remote OpenOCD debugging, Could not verify ST device!

i already did this in 2021 https://community.st.com/t5/stm32-mcus-products/openocd-not-reseting-my-chip/td-p/192537Is there a chance ST implemented new anticlone stm32 chips in new cubeIDE versions? and noone told OpenOCD about it?Using CUBEIDE 1.16....

Javier1_0-1748433666210.jpeg Javier1_1-1748433666278.png
Javier1 by Principal
  • 1866 Views
  • 3 replies
  • 0 kudos

STM32L4S5VIT6 STOP2 Mode Wake-Up Issue in Release

Hello STM32 Community,I'm working with the STM32L4S5VIT6 microcontroller and implementing low power functionality using STOP2 mode. Setup Summary:I use a GPIO button (external interrupt) to enter STOP2 mode on the first press.On the second press, I a...

Gohil by Associate II
  • 764 Views
  • 1 replies
  • 0 kudos

Input capture frequency overflow handle

Good afternoon community,I am trying to capture the frequency which is given by wave-form generator and i am able to capture that,But issue is i am not able to capture when it is face the underflow condition and it will not working properly.please su...

MG1 by Associate II
  • 4384 Views
  • 5 replies
  • 0 kudos

STM32G473 Debugger bug

Hello,i have a project created with STM32Cube IDE Version 1.18.1 for the STM32G473CCU micro-controller with 256k flash. My binary file is 180k length and the debugger launched from STM32Cube fails to program the flash because it enables the dual bank...

Leo4 by Associate II
  • 639 Views
  • 0 replies
  • 0 kudos

function macro usage issues in stm32cubeIDE

Hello,        I have some issues with function macros usage in my stm32cubeIDE project after importing some generated code in cubeIMX.      This issues come on the back of my work related to this topic : is there any sample for X-NUCLEO-NFC08A1 to be...

Copilot integration with CubeIDE 1.18

STM IDE 1.18.From Marketplace I select copilot 0.6.0.Installation fails, missing dependecies.On Eclipse Embedded 2025-06 works perfectly.Do I have to migrate my projects to Eclipse Embedded?Best Regards 

FMarr.2 by Associate III
  • 2061 Views
  • 2 replies
  • 0 kudos