STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1093 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 476 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Choose different builds for "Run" and "Debug" button

Currently the behaviour of CubeIDE is to always choose the same build configuration for the Run and Debug button.Is there a way to have the two seperated? Most of the time I want to flash the Debug build for debugging and the Release build with stron...

A.D. by Senior
  • 2545 Views
  • 3 replies
  • 2 kudos

STM32CubeIDE on openSUSE Tumbleweed

Hello,I try to get STM32CubeIDE working on openSUSE Tumbleweed. But the application won't start due to some error.The log files I have attached. Does someone have an idea or experience with this OS?

MBabu.3 by Associate II
  • 350 Views
  • 1 replies
  • 0 kudos

custom objcopy command

Is it possible to edit the objcopy command emitted by the Stm32CubeIDEIDE? I need to make some adjustments to keep some RAM addresses from showing up in the hex file. Advice on the internet seems to thing this is easily adjustable in the IDE. However...

Carl_G by Senior III
  • 349 Views
  • 1 replies
  • 0 kudos

Resolved! Build Analyzer issue

Hello,Is there a trick to get the Build Analyzer to produce data every time the code is compiled?   It seems like the only way I can get it to update the window is if I change something in the linker script file and recompile again.   Is there an eas...

matt-crc by Senior III
  • 10033 Views
  • 21 replies
  • 10 kudos

Debugger Stopped

Nucleo-WL55JC1CubeIDE 1.18.1STM32CubeIDEVersion: 1.18.1Build: 24813_20250409_2138 (UTC)OS: Windows 11, v.10.0, x86_64 / win32Java vendor: Eclipse AdoptiumJava runtime version: 21.0.3+9-LTSJava version: 21.0.3This board has the debugger built in.  Thi...

jlaiosa by Associate II
  • 384 Views
  • 0 replies
  • 0 kudos

CAN alternate functions *NOT* configured in stm32IDE

Trouble Report: STM32G474 FD CAN RX Interrupt Causes HardFault Due to VTOR Left at 0x00000000 Platform Details----------------- Microcontroller: STM32G474VETx- IDE: STM32CubeIDE- Version: 1.16.0- Build: 21983_20240628_1741- Startup project: Standard ...

rclar.6 by Senior
  • 1174 Views
  • 6 replies
  • 0 kudos

STM32F415 SDIO + STOP Mode

I am using an SD card with STM32F415. The MCU periodically enters STOP mode.Currently, I observe the following behaviour in the IDE related to SDIO:- Before enabling SDIO for the first time, the current consumption in STOP mode is as expected (around...

stm32f415-clock.png
MZadn.2 by Associate II
  • 614 Views
  • 2 replies
  • 0 kudos