cancel
Showing results for 
Search instead for 
Did you mean: 

No way to Log into MyST on CubeIDE V 18 ??

Ricko
Senior III

Hi,

I upgraded CubeIDE to V.18 but when creating a project from an IOC file it could not generate any code because the micros packages are missing. It said to log into MyST but there is no Login option where it previously was (see screenshot below).

How do you do that in V18?

Thank you

 

Ricko_0-1741031489011.png

 

1 ACCEPTED SOLUTION

Accepted Solutions
Semer CHERNI
ST Employee

Hello @Ricko

First let me thank you for posting.

In fact ,since the STM32CubeIDE 1.17.0 ,the way to log in was modified and it's as you mentioned under "Help -> STM32Cube Updates -> Connection To My ST"

BR,
Semer.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
TDK
Super User

Try Alt+L

If you feel a post has answered your question, please click "Accept as Solution".

Thank you @TDK 

no that does not work but I just found out that it is under Help -> STM32Cube Updates -> Connection To My ST

Semer CHERNI
ST Employee

Hello @Ricko

First let me thank you for posting.

In fact ,since the STM32CubeIDE 1.17.0 ,the way to log in was modified and it's as you mentioned under "Help -> STM32Cube Updates -> Connection To My ST"

BR,
Semer.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.