cancel
Showing results for 
Search instead for 
Did you mean: 

WRP2A and WRP2B registers are not showing on the SFRs tab

CTapp.1
Senior III

I'm working on a project that's using an STM32G484CEUX. The WRP2A and WRP2B registers are not showing under the FLASH peripheral of the SFRs tab:

CTapp1_0-1741012250759.png

The device is running is dual bank mode.

I have added them to the .svd file, but I think they should already be there?

Edited to correct grammar.

All posts are made in a personal capacity
MISRA C++ Chair
MISRA C WG Member
Director The MISRA Consortium Limited (TMCL)
1 ACCEPTED SOLUTION

Accepted Solutions

Hello @CTapp.1 ,

Thank you for bringing this issue. 

It has been reported to STM32CubeIDE development team.

Internal ticket number:  204474 (This is an internal tracking number and is not accessible or usable by customer)

Thanks.

Mahmoud

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
Mahmoud Ben Romdhane
ST Employee

Hello @CTapp.1 ,

First let me than you for posting.

For more investigation, I suggest that you provide the STM32CubeIE Version.

Thanks.

Mahmoud

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

CTapp.1
Senior III

Sorry, I meant to add that. I am using 1.17.0.

 

All posts are made in a personal capacity
MISRA C++ Chair
MISRA C WG Member
Director The MISRA Consortium Limited (TMCL)

Hello @CTapp.1 ,

Thank you for bringing this issue. 

It has been reported to STM32CubeIDE development team.

Internal ticket number:  204474 (This is an internal tracking number and is not accessible or usable by customer)

Thanks.

Mahmoud

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.