STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1406 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 556 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

STM32Cube IDE getting slow compilation

Case Description: Dear All,My STM32Cube IDE taking lost of time to compile to code previously it was taking 20sec only but now it taking 10 min and compile 20% code, please suggest what the issue,CPU - I7RAM - 16 CPU Utilization - <30%RAM utilization...

vchau.2 by Associate III
  • 1616 Views
  • 6 replies
  • 1 kudos

Not able to configure Google tests with STM32Cube IDE

I have installed STM32Cube IDE and created project successfully.Generated basic programming and tried to create google test to create test cases. But while creating C/C++ Unit under C/C++ tests getting error in C/C++ application in Main tab.Attached ...

SasiSree by Associate
  • 596 Views
  • 3 replies
  • 1 kudos

SAI Function call generates unexpected data stream

Hello Board,I hope you are all having a great summer. I am currently trying to configure the 144 devolopment board with the STM32H723zg chip, to run the built in SAI peripheral. Specifically I want to transmit a frame of 256 bits, with 16 slots and s...

Kewin_J_0-1754294935646.png Kewin_J_1-1754294961236.png Kewin_J_2-1754294984806.png Kewin_J_3-1754295150919.png
Kewin_J by Associate II
  • 526 Views
  • 1 replies
  • 0 kudos

Resolved! How to produce list of pin assignments?

Hello, all,I'm using STM32CubeIDE to design my first STM32 micro-controller circuit. I've used the tool to assign functions to about 20 pins on the micro-controller so far. Now, I'm at the stage where I'm creating the schematic and connecting externa...

KevinZ by Associate III
  • 6105 Views
  • 4 replies
  • 2 kudos

Resolved! Break at address "0x8000B2C" with no debug information

Hi all,I followed this STM32CubeIDE tutorial to debug an STM32H7S3L8 project running from external flash (OSPI NOR). After flashing and starting the debug session, I get the following error:Break at address "0x8000B2C" with no debug information avail...

Duc by Senior
  • 911 Views
  • 4 replies
  • 0 kudos