STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1549 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 587 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

I have stm32H74Zi chip and is running in 64Mhz clock speed and have scaled down the speed to 32Mhz for APB1 (I2C peripheral) using clock divider. Want to know how TIMINGR value is working with both the frequencies (32 and 64Mhz at APB1 peripheral).

Using clock divider(/2) scaled down the APB1 peripheral clock speed to 32Mhz. Now I have different TIMINGR values for for each of 32 and 64MHz clock speed at APB1. I tried 32MHz TIMINGR value for 64MHz clock speed and it worked.I want to know how the...

Umahe.1 by Associate II
  • 1399 Views
  • 2 replies
  • 0 kudos

How to support multiple STM targets in a project

Hello,From time to time it is good to be able to target multiple STM devices for a project. In our case we are evaluating a number of chipsets and have eval boards for the various chips. What I want to do is to be able to generate a project which wil...

Resolved! CUBE IDE and code style checker

Hi folks,STM32CubeIde /eclipse comes with a code style checker. I just ran it. The default settings do not cover ST's code style. Is it possible to get a config file so CubeIde automatically checks for STM32s coding guidelines?Is ST development team ...

STM32cube problem with Migrate FW version

Hi, I have a project STM32F429-DISC1 with BSP libraries created in CubeIDE and everything works but when I give Migrate the project from old FW V1.24.2 to last V1.26.2 the display stops showing. Has anyone already solved what the problem may be? If I...

Filipx.87 by Associate II
  • 2440 Views
  • 4 replies
  • 0 kudos

Rules for Project from makefile?

So there is the menu option :File > New > Makefile Project with Existing CodeWith this structure:Top----+----Folder----+---- makefile | +---- other files & folders | ...

Why do I get "Failed to insert all hardware breakpoints: You may have requested too many..." even when I have NO breakpoints/watchpoints set?

I am running 1.4.0 on a VM on a windows10 machine and trying to work with "Nucleo-L433RC-P". The error is not totally consistent. Sometimes it allows one breakpoint to be hit, sometimes it complains about the only breakpoint and stops (one time only...

warm38 by Associate III
  • 2879 Views
  • 1 replies
  • 0 kudos