STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1549 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 587 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

STM32F768I-DISCO unable to run or debug

So I recently purchased an STM32F768I-DISCO board and every time I try to run or debug a code, I get "The selection cannot be launched, and there are no recent launches�?. I do not get any build errors so it I believe it has something to do with the ...

JTurn.2 by Senior
  • 1524 Views
  • 2 replies
  • 0 kudos

hard fault error occur

I use the STM32F100RB and make a bootloader.​The PC is connected to the STM32F100RB via UART, and the program to be executed is sent from the PC and extracted to the internal RAM. However, when the program is executed in the RAM, hard fault error occ...

0693W00000Hp8YVQAZ.png
Myasu.1 by Senior
  • 1186 Views
  • 2 replies
  • 0 kudos

Resolved! STM32CubeIDE after installing on debian is nowhere to be found

It is Debian based distio (crunchbang plusplus), after installing IDE using sh script provided, the IDE is found in the list of programs, but it is not in the PATH, and I could not find location of the installed files. Also attempting to run installa...

TMark.14 by Associate III
  • 3816 Views
  • 4 replies
  • 0 kudos

Hi, I hope I hit the correct subforum. I cannot update STM32CubeIDE to version 1.8.0. When trying to update, I get the following error message:

An error occurred while collecting items to be installedsession context was:(profile=STM32CubeIDE, phase=org.eclipse.equinox.internal.p2.engine.phases.Collect, operand=, action=).No repository found containing: osgi.bundle,com.st.stm32cube.common.mx,...

AAnth.1 by Senior
  • 1605 Views
  • 2 replies
  • 0 kudos

Cannot import System Workbench project

Project works in System Workbench for STM32 - Version: 1.17.0.201812190825When attempting to import into STM32CubeIDE Version 1.7.0, this popup appears:OK, fine - I pick the correct MCU.Then the same popup appears...At this point, it doesn't matter i...

0693W00000Dm3IQQAZ.png
inojosh by Associate III
  • 3170 Views
  • 6 replies
  • 0 kudos