STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1549 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 587 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! How do I debug an externally built executable?

I built an elf executable for the STM32H743ZI. I did not create this executable from within STM32CubeIDE. Still, I would like to debug it from within STM32CubeIDE. How do I load the elf file in the STM32CubeIDE and debug the executable on a target (S...

AIsma by Associate II
  • 7972 Views
  • 5 replies
  • 0 kudos

STM32IDE: Don't open source when stopping debugging session

This maybe a silly question, but is it possible to set the IDE NOT to open the source file when stopping or pausing a debug session.Nine times out of ten, it stops in a core routine and one just ends up with lot of open files that are generally of li...

AJJ by Associate II
  • 2358 Views
  • 2 replies
  • 0 kudos

Where do I download the GNU Tools for STM32?

This reply to this post claims there used to be a way to download this, but now ST removed the ability to download their patched toolchain? https://community.st.com/s/question/0D50X0000BQOoj5/difference-between-the-toolchain-gnu-tool-for-stm32-and-gn...

Jb.161 by Associate
  • 4302 Views
  • 1 replies
  • 0 kudos

Errors in the configurator of the STM32CubeIDE for microcontroller STM32L100RB. (Not observed for STM32F103, etc.) (Low Layer only)

Ubuntu STM32CubeIDE 1.8/1.7File -> New -> STM32 ProjectChoose STM32L100RB -> Next -> Project Name : "removeMe2" -> FinishIn Device Configuration Tool:  Pinout&Configuration -> Connectivity -> SPI1 -> Mode: Full Duplex Master  Project Manager -> Advan...

ATret.3 by Associate III
  • 2645 Views
  • 1 replies
  • 0 kudos

Resolved! STM32CubeIDE missing pin labels

using: NUCLEO-H745ZI-Q board, STM32CubeIDE: Version: 1.8.0 Build: 11526_20211125_0815 (UTC)I am new to STM32 and trying to do a simple led/gpio test.can't identify a pin since there is no label that converts from port and pin, saw at some tutorials t...

HZz.1 by Associate
  • 2541 Views
  • 2 replies
  • 0 kudos

Why my program doesn't compile using LwIP?

I'm trying to compile my program, but it doesn't work due to an error probably related to LwIP includes.In file included from c:\st\stm32cubeide_1.6.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.wi...

0693W00000ANAYJQA5.png
Jvan .10 by Associate III
  • 2212 Views
  • 2 replies
  • 0 kudos

Resolved! No such file or directory ?

Hi guys! I have a trouble about STMCubeIDE, I installed and created a project, Later, I received this two error ; c:\st\stm32cubeide_1.8.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_2.0.0.20...

bnymntrz by Associate III
  • 7026 Views
  • 3 replies
  • 0 kudos

Resolved! Weird STMCubeIDE debug behavior - global structs showing up as all zeros but the code acts as it they are populated with data as they should be!

I have a project on an STM32F4 that consists of a Bootloader and Main application. Both of these apps read an external Flash to retrieve configuration data. The Bootloader is looking to see if Main had previously uploaded new FW to the Flash and if...

MStra.3 by Associate III
  • 1397 Views
  • 1 replies
  • 0 kudos

STCUBE hogs whole screen width

Hello,I run an a laptop with an additional screen at the side. stcube starts up hogging all the available with and exact the middle, where there is a gap. Most other application behave more sensible. I would appreciate if stcube would do so too.

Resolved! STM32CubeIDE Black Theme Problem

I don't find any options to change the font color for some files like linker scripts (for C/C++ Files it's ok). It's very difficult to read the file and i would like to use the dark theme.Same thing for not included code : Maybe one of you is aware o...

0693W00000HoeQSQAZ.png 0693W00000Hof5QQAR.png
AdrienC by Associate
  • 3348 Views
  • 4 replies
  • 0 kudos