STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1549 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 587 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Problem uploading code in custom board.

Hi I designed a custom board based on the STM32G030K8 MCU, I was able to upload my code on the device successfully and the device was working fine, I updated the code a few times and was able to successfully upload the code to the board. However I di...

0693W00000Hq06NQAR.png
APant.1 by Associate II
  • 3814 Views
  • 4 replies
  • 0 kudos

STM32Cube. Fail to start GDB server

When I try to flash the stm32G pops up the error "fail to start GDB server.Looking on internet.I have found in the form that a cos.of this error could be Avast antivirus, but even if i have uninstalled it, does not solve my issue.​

FTrom by Associate II
  • 854 Views
  • 0 replies
  • 0 kudos

LWIP over USB with stm32CubeIDE

Hi,Create an http server using ETH and LWIP middleware is easyI would like to use LWIP but using USB_OTG.Do you plan to implement such solution, or does it exist an example of implementation ?Thanks

STM32CubeIDE v1.8 and Live Expressions

Please, help me to fix this problem: when I debugging STM32 MCU with J-Link in STM32CubeIDE v1.8 it is not possible to change the Live Expressions tab values 'on the fly' (while MCU is running). The error message is on the pic.

ivainc by Associate III
  • 8029 Views
  • 5 replies
  • 0 kudos

Remote debugger

Hi,I'm looking for a solution to debug a device with remote access.Meaning, the device and an emulator will be in location A and code project will be in a location B. It's prohibited to run the code project IDE on the location A.Device uses STM32F4.A...

ari_v2 by Senior
  • 1354 Views
  • 2 replies
  • 0 kudos