STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1413 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 558 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Storing and retrieving an STM32CubeIDE project in GitHub

I have a project (https://github.com/carlk3/Digital-Automotive-Generator-Voltage-Regulator) that I've been developing in STM32CubeIDE on (Ubuntu) Linux. Now I want to move it to STM32CubeIDE on Windows. I'm using GitHub for source code management (SC...

CKugl.1 by Senior II
  • 3369 Views
  • 3 replies
  • 0 kudos

Hi! I have installed STM32CubeIDE and I created new project on Nucleo F411RE board but I can't compile this project. I will add that this is a blank project (I didn't write any line of code).

I tried uninstalling the program and reinstalling it but it didn't work. Can somebody help me? I have this output in my console:19:05:11 **** Incremental Build of configuration Debug for project Test ****make -j4 all arm-none-eabi-gcc "../Drivers/STM...

PŁucz.1 by Associate II
  • 4448 Views
  • 9 replies
  • 0 kudos

Resolved! File are not modified when using Git with STM32Cube IDE

Hello everyone, I'm fairly new to Git and I'm trying to use it as my firmware version manager for an existing STM32 project. I set up correctly my project directory to work on my computer and with Bitbucket and everything works fine. I created a new ...

XB1 by Associate II
  • 3306 Views
  • 6 replies
  • 0 kudos

STM32H735G-DK: Device in lock up state, possibly "read and debug" protected. Use monitor commands to remove the protection // Failed to execute MI command: load

HelloI have:1. STM32CubeIDE (Version: 1.10.1, Build: 12716_20220707_0928)2. STM32H735G-DK boardI have tried running a demo from TouchGFX app (4.20) and it flashes and run well, but I have a problem with running 'FreeRTOS' example created in 'Example ...

VBout.2 by Associate II
  • 958 Views
  • 0 replies
  • 0 kudos

not a custom to non make files, how do I add my source files?

using CUBE IDE here.I see how to add other header paths but I'm sure I need to tell the compiler I made a new folder off of src and for it to add my source files. Is there a way to tell the linker I have another c file?under the source location , I c...

ulao by Associate III
  • 1201 Views
  • 1 replies
  • 0 kudos

Live Expression stopped working "Failed to evaluate expression" For 2 years I have been using STM32CubeIDE debugging with Live Expression view without any problems. Starting Oct 2022 I only get "Failed to...."

This only happens to new variables added to my C code after Oct 2022. "Old" variables still work fine. When I add failing variables to the "Expression" tab I get "Error: Multiple errors reported". Reported are: Multiple errors reported.1) Failed to e...

wvan .1 by Associate
  • 5395 Views
  • 7 replies
  • 0 kudos