STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1554 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 588 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! STM32G0 bought with level 2 protection

Hi all, I'm new to this STM32 community.I have a small problem: I bought some STM32G0P0.. for my project, also making the PCB and the rest. But after soldering the various components, I try to program one and see that the level 2 protection is active...

0693W00000WIxGqQAL.png 0693W00000WIxHFQA1.png

How to debug main.cpp imported from mbed and visualize the contents of variables

�?�在�?�ステータス:I次�?�図�?�示�?�よ�?��?��?2 �?��?�ヘッダー ファイル�?� 1 �?��?� cpp ファイルを mbed �?�ら Core/Src �?�イン�?ート�?��?��?��?�。�?��?��?��?cppコードをコンパイル�?�る�?��?無数�?�エラー�?�発生�?��?��?�。知り�?��?��?��?�ヘッダーファイル�?��?�る場�?��?�?��?��?�れ�?�デ�?ッグ�?��??�?��?��?�?エラーを解決�?�る...

0693W00000Y6uMkQAJ.png 0693W00000Y6uMuQAJ.png 0693W00000Y6uNOQAZ.png
hsanr.1 by Associate II
  • 2378 Views
  • 3 replies
  • 0 kudos

I am trying to run some applications on STM32 through the STMCubeIDE. Just wanted to know if there is any API which can be used inorder to perform the same functions using CLI.

The overview of the workflow is as follows: Open the STMCubeIDE -> Open new Project -> elect the directory -> Build -> debug -> buildSo I am looking for a python library/API which can be used to perform the same function through Automation. The UI au...

VNaga.2 by Associate II
  • 4613 Views
  • 9 replies
  • 0 kudos

How to add a .lib file to a project?

Hello,I have recently bought an evaluation board. The manufacturer provides a library and a Keil sample project, but I would like to integrate the library in a STM32 Cube project.I found on the internet how to add a .lib file (www.eclipse.org/.../), ...

Inigo by Associate II
  • 10656 Views
  • 6 replies
  • 0 kudos

Resolved! How to share libs between projcts, same workspace.

I developed some libs to control a custom LCD.At the beginning the workspace only had one project, 01_main, and files related to my lcd and driver were located there, later I started another project 02_rtos, so I copied LCD files into new project.I n...

0693W00000Y7ERpQAN.png 0693W00000Y7EMfQAN.png 0693W00000Y7ENJQA3.png
dhs by Senior
  • 1932 Views
  • 4 replies
  • 0 kudos