cancel
Showing results for 
Search instead for 
Did you mean: 

How can you validate that Independent WatchDog (IWDG) is resetting the processor ?

mm.51
Associate II

Development Board: Nucleo-L476RG.

IDE version: STM Cube IDE 1.11.0

I have implemented this

"Configuring the IWDG when the window option is disabled When the window option it is not used, the IWDG can be configured as follows:

1. Enable the IWDG by writing 0x0000 CCCC in the IWDG key register (IWDG_KR).

2. Enable register access by writing 0x0000 5555 in the IWDG key register (IWDG_KR).

3. Write the prescaler by programming the IWDG prescaler register (IWDG_PR) from 0 to 7.

4. Write the IWDG reload register (IWDG_RLR).

5. Wait for the registers to be updated (IWDG_SR = 0x0000 0000).

6. Refresh the counter value with IWDG_RLR (IWDG_KR = 0x0000 AAAA)."

I'm not sure as to how I can validate that my processor is resetting.

Any suggestions would be appreciated.

Thanks

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Pavel A.
Super User

> how I can validate that my processor is resetting

Start the IWDG and don't refresh it (just spin) for a few minutes.

The MCU should reset. In your main() function read the reset reason and check that it is because of IWDG:

  uint32_t reset_flags = RCC->CSR;
  if (reset_flags & RCC_CSR_IWDGRSTF) {
    // This was IWDG 
  }
  else if (reset_flags & RCC_CSR_WWDGRSTF) {
    // This was WWDG
  }
  else if (reset_flags & RCC_CSR_SFTRSTF) {
    // Software reset (NVIC_SystemReset or by debugger)
  }

View solution in original post

2 REPLIES 2
MM..1
Chief III

In main code start read reset flags and clear it.

Pavel A.
Super User

> how I can validate that my processor is resetting

Start the IWDG and don't refresh it (just spin) for a few minutes.

The MCU should reset. In your main() function read the reset reason and check that it is because of IWDG:

  uint32_t reset_flags = RCC->CSR;
  if (reset_flags & RCC_CSR_IWDGRSTF) {
    // This was IWDG 
  }
  else if (reset_flags & RCC_CSR_WWDGRSTF) {
    // This was WWDG
  }
  else if (reset_flags & RCC_CSR_SFTRSTF) {
    // Software reset (NVIC_SystemReset or by debugger)
  }