STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1427 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 558 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! STM32H723ZG USB CDC ADC DMA

I am using STM32H723ZG nucleo board. When I enable HAL_ADC_Start_DMA(&hadc1, (uint32_t*)adc_buf, ADC_BUF_LEN); USB Virtual port doesn't show up and when I disable it, it shows up. Can anyone explain what could be the issue?I was able to print "Hello"...

AKhot1_0-1693307526832.png AKhot1_1-1693307704147.png AKhot1_3-1693307747447.png
AKhot.1 by Senior
  • 3037 Views
  • 4 replies
  • 0 kudos

Help using SWD and NRST as GPIO safely - STM32G031

Hi, so I've chosen to use STM32G031J6M6 8-pin version for an audio level meter project to get me started. I'm using pin 1 as the adc input, 2 and 3 are 3v3 and gnd, obviously. I was hoping to use the remaining 5 pins as GPIO outputs attached to LEDs ...

NGD by Associate II
  • 9552 Views
  • 11 replies
  • 1 kudos

STM32CubeIDE Mass Erase rather than Sector Erase

I have a STM32H723 on a custom board that I'm having a lot of trouble programming. Every time I try to flash it, the erasing of flash sectors fails. I can, however, perform a full chip erase. All the option bytes are configured as they should be, but...

Iris-DM by Associate III
  • 2430 Views
  • 1 replies
  • 0 kudos

Hard Fault handler FFT

After the arm_fft function, I am running into a hard fault handler when running in debug mode. I am not getting why is it happening. Please help with this. Is it because of some wrong memory allocation? 

AKhot1_0-1693225742548.png
AKhot.1 by Senior
  • 3461 Views
  • 6 replies
  • 0 kudos

start stm32

I wrote a program with buttons and LEDs.I wanted to continue with other peripheral devices. But unfortunately I had to reinstallWindows. And the problems started: I can neither open the previous project nor make a new one. STM32 Cube needs to be upda...

STM32WB LPSLEEP issue

Hello, I'm trying to implement Low power sleep on STM32WB. The sequence is as per LPSLEEP example:HAL_PWREx_EnableFlashPowerDown(PWR_FLASHPD_LPSLEEP); SystemClock_Decrease(); //MSI 2MHZ HAL_SuspendTick(); HAL_PWR_EnterSLEEPMode(PWR_LOWPOWERREGULATOR_...

MHast.1 by Associate II
  • 1620 Views
  • 1 replies
  • 0 kudos

TM32CubeIDE 1.13.1 and Nucleo-F429ZI - Linker Error

Hello,when I create a new project with Ide 1.13.1 and Nucleo-F429ZI and enable ETH,  LWIP and HTTPD then I get following linker errors. Seems some module are not compiled automatically. What could be the reason? How to solve?C:/ST/STM32CubeIDE_1.5.0/...

jens3 by Associate
  • 2054 Views
  • 2 replies
  • 0 kudos

Debugger wont launch

I've been using the STM32CubeIDE on a Ubuntu system to develop code for our STM32 based device. Up until today everything was working just fine. But today I made some changes to my code, and when I went to launch the debugger to try it out, I get n...

DTovey by Associate II
  • 9827 Views
  • 12 replies
  • 12 kudos