User Activity

MCU: STM32L4R9ZGJ6Hardware: Custom battery powered boardLED: ARGB1313HSDesired LED functionality: Blink, on/off, fade in/out ("Breathing")Hello,I am familiar with a regular timer and how they can drive a RGB LED using multiple channels (CCx registers...
Details:MCU: STM32L4R9ZGJ6IDE: STM32CubeIDE v1.6.1SDK: STM32Cube_FW_L4_V1.14.0Board: Custom PCBHello,I am seeing really strange behavior where bits 31-24 in the RCC->CSR register are usually always 0. I have verified this behavior on two boards. The ...
BackgroundHardware:STM32L4R9ZGJ6 (1 MB flash)Custom boardSoftware:STM32CubeIDE v1.6.1STM32CubeProgrammer v2.8.0Hello,I have a couple questions.Question 1: What is the difference between the user configuration option bits DB1M and DBANK?According to t...
Some Background:MCU: STM32L4R9ZGJ6SDK: STM32Cube_FW_L4_V1.14.0Programmer: STM32CubeProgrammer v2.2.0External Flash: OSPI (MT35XL512ABA1G12)Application IDE: STM32Cube IDE 1.6.1External Loader IDE: Keil uVision 5.16aProject is was started on the STM32L...
Hello,Some background:STM32CubeIDE 1.6.1MCU: STM32L4R9ZGJ6SDK: STM32Cube_FW_L4_V1.14.0 (Yes I know it's old ~ 2019) Project is too large to update at the moment.I am currently debugging external DAC audio issues. I reverted to using simple SAI blocki...
Kudos from