STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1447 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 566 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Query related to Debug folder

Is it possible to get the .o files i.e. the output files in the same folder because whenever I build the code the output files gets saved in the Debug folder. 

Monika_02_0-1690539104679.png
Monika_02 by Associate II
  • 3552 Views
  • 5 replies
  • 1 kudos

Resolved! HSI48 on STM32F072C8T problem

Hello,I have a problem with a clock configuration on my STM32F072C8T6. I need the 48MHz clock (HSI48) for the onboard USB communication. I have enabled this via ioc in the clock configuration. Everything looks fine there and no conflict is reported.N...

Touby by Associate II
  • 14795 Views
  • 14 replies
  • 3 kudos

Resolved! Debug Error on Dual Core STM34H747I-DISCO Board

Using Application Note AN5361 and a Online ST Video. I have create a project in STM32CubeIDE for the STM32H747I-Disco Board. As a test of the debugging, I have have both cores simply blinking separate LEDs.I set up the CM7 debug configuration  per AN...

SLimi1_0-1691289197359.png
SLimi.1 by Associate III
  • 2599 Views
  • 3 replies
  • 0 kudos

Keil MDK to STMCube IDE project conversion

Hi.Bought the Arm Education Media book "DSP using Arm Cortex-M based Microcontrollers" along with the SMP32F407G-DISC1 board and the LTEK audio board. Got the LTEK audio loop thru example working under Keil.Now trying to get this project working unde...

waddy by Associate II
  • 1703 Views
  • 0 replies
  • 0 kudos

How to operate STM32 power on off

We implemented a lwip tcp server with STM32 and even sent and received messagesBut when I was debugging, it was good I'm trying to disconnect ST-LINK and see if it works by turning the power on and off without debugging, but the server didn't even cr...

ark2 by Associate III
  • 2052 Views
  • 2 replies
  • 0 kudos

Use LWIP in C++ main file

Hi every oneHow can I use LWIP TCP connection(socket, NetConn, Raw ... )  in main.cpp   ?I can use Raw in main.c properly but I need to use it in cpp files. thank you

MTora.1 by Associate III
  • 1060 Views
  • 0 replies
  • 0 kudos