STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1425 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 558 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Code performance profiling

Hello,Is there an integrated tool in STM32CubeIDE that I can use to measure how long a block of code lasts?I was used to use a similar tool on TI CodeComposer, that measured the elapsed clocks from a breakpoint to another.Thank you,Carlo

CTabo.1 by Senior
  • 4846 Views
  • 2 replies
  • 0 kudos

Resolved! error: unknown type name '__root'

I am using below codes. But this define not supportted #define KeepInCompilation __root #define KeepInCompilation __root   /* Private function prototypes -----------------------------------------------*/ int Init (); KeepInCompilation int Write (uin...

0693W00000KbyTvQAJ.png

Target is not responding, retrying.. Issues ?

Hai.....,I am using STM32H743IIT6 custom Board and CubeIDE. Run the code after download it showing "Target not responding retrying......." and again try to download the same code in MCU i couldn't download, It show "Error in initializing ST-LINK de...

GMano.1 by Associate II
  • 21831 Views
  • 4 replies
  • 0 kudos

Resolved! Branch with link instruction doesn't jump to main

Hi,I'm working with a STM32G491KEU (512KB Flash).I use a custom bootloader so the startup in the printsreen is from the application. The MCU will first start in the custom bootloader and then it should change to the application.It reaches the startup...

Mat1_1-1695223672584.png Mat1_0-1695297751792.png
Mat1 by Associate III
  • 1556 Views
  • 1 replies
  • 0 kudos

Resolved! Mixed use of HAL and LL driver functions

Hello,I have a project where I use both HAL and LL functions, on different files, for different funcitions.As described in UM2319, I defined both USE_HAL_DRIVER and USE_FULL_LL_DRIVER as compiler preprocessor symbols.In this case I have an error indi...

CTabo.1 by Senior
  • 5473 Views
  • 6 replies
  • 2 kudos

Query related to Debug folder

Is it possible to get the .o files i.e. the output files in the same folder because whenever I build the code the output files gets saved in the Debug folder. 

Monika_02_0-1690539104679.png
Monika_02 by Associate II
  • 3527 Views
  • 5 replies
  • 1 kudos

Resolved! HSI48 on STM32F072C8T problem

Hello,I have a problem with a clock configuration on my STM32F072C8T6. I need the 48MHz clock (HSI48) for the onboard USB communication. I have enabled this via ioc in the clock configuration. Everything looks fine there and no conflict is reported.N...

Touby by Associate II
  • 14655 Views
  • 14 replies
  • 3 kudos